7EN02-0468-01

Telegram information for data records

The following sections outline the telegram information used in data records. The tables contain the following information (if applicable):

  • Data format in hex (for example, 16-bit integer)

  • Primary VIF in hex

  • Primary VIFE codes in bin and hex

  • Manufacturer-specific VIFE codes in bin and hex

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?