7EN02-0468-01

Setting up baud rate

The Modbus (iEM2455) baud rate can be set from 1200 to 38400. The M-bus (iEM2435) baud rate can be set from 300 to 9600.
To change the baud rate, follow these steps:
  1. Scroll with the buttons to Program mode 3 (Pro-3).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Enter the 4 digit password (default: 0000): scroll with the buttons and select each digit 0 – 9, hold the up-arrow button for 3 seconds to confirm each digit.
  4. Scroll to baud rate (bAUd) page.
  5. Hold the up-arrow button for 5 seconds to enter program mode.
  6. When the value starts blinking, select:
    • Modbus (iEM2455): 1200 / 2400 / 4800 / 9600 / 19200 / 38400

    • M-Bus (iEM2435): 300 / 600 / 1200 / 2400 / 4800 / 9600

  7. Hold both buttons for 3 seconds to confirm the new setting.
  8. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?