7EN02-0468-01

Energy consumption LEDs

The two red LEDs on the front panel indicates the energy consumption. When power is consumed, the LEDs flash. When more power is consumed, the LEDs flash at a faster rate.

The reactive energy consumption LED (A=10000 imp/kVARh) flashes during reactive energy consumption and the active energy consumption LED (B=10000 imp/kWh) flashes during active energy consumption. The LEDs flash at 10000 imp/kWh.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?