7EN02-0468-01

Configuring the meter using the M-Bus tool

You can use the M-Bus tool to configure basic meter settings.
  1. Select Setup > Config to switch to configuration mode.
  2. Set the values that you want to change, then click Send for that value or section.

    Some values may be unavailable based on existing settings.

    The configuration screen has the following sections:

    Section

    Description

    Set Baudrate

    Set the baud rate.

    Set Address

    Set the meter address.

    Reset

    Reset partial energy and input metering accumulations.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?