7EN02-0468-01

Setting up Modbus ID (iEM2455) / M-Bus ID (iEM2435)

The Modbus ID (iEM2455) can be set from 001 to 247. The M-Bus ID (iEM2435) can be set from 000 to 250.
To change the Modbus ID (iEM2455) / M-Bus ID (iEM2435), follow these steps:
  1. Scroll with the buttons to Program mode 2 (Pro-2).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Scroll to Modbus ID (iEM2455) / M-Bus ID (iEM2435) (M-Id) page.
  4. Hold the up-arrow button for 5 seconds to enter program mode.
  5. When the value starts blinking: select 3 digits (Modbus (iEM2455): 001 – 247 / M-Bus (iEM2435): 000 – 250).
  6. Hold both buttons for 3 seconds to confirm each digit.
  7. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?