7EN02-0468-01

Adding / removing registers to / from automatic scroll

  1. Scroll to the register that you need to add or remove.
    NOTE: Only the registers in the sub-menu after the total active energy, total reactive energy, active power and Program mode 1 can be added or removed to / from the automatic scroll. Total active energy cannot be removed.
  2. Hold the up-arrow button for 5 seconds to add or remove the register.
  3. The LCD displays in OK or out OK.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?