7EN02-0468-01

Energy and energy by tariff

Energy values - 64-bit integer

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

Total energy (cannot be rest)

0x0C84

3205

0x0C83

3204

R

4

Int64

Wh

Forward active energy

0x0C88

3209

0x0C87

3208

R

4

Int64

Wh

Reverse active energy

0x0C8C

3213

0x0C8B

3212

R

4

Int64

Wh

Total active energy

0x0C94

3221

0x0C93

3220

R

4

Int64

VARh

Forward reactive energy

0x0C98

3225

0x0C97

3224

R

4

Int64

VARh

Reverse reactive energy

0x0C9C

3229

0x0C9B

3228

R

4

Int64

VARh

Total reactive energy

Partial energy

0x0CB8

3257

0x0CB7

3256

R

4

Int64

Wh

Forward partial active energy

Energy by tariff

0x105F

4192

0x105E

4191

R/WC

1

UInt16

-

Tariff

  • 01: T1 (default)
  • 02: T2

0x1064

4197

0x1063

4196

R

4

Int64

Wh

T1 Forward active energy

0x1068

4201

0x1067

4200

R

4

Int64

Wh

T2 Forward active energy

0x106C

4205

0x106B

4204

R

4

Int64

Wh

T1 Reverse active energy

0x1070

4209

0x106F

4208

R

4

Int64

Wh

T2 Reverse active energy

0x1074

4213

0x1073

4212

R

4

Int64

Wh

T1 Total active energy

0x1078

4217

0x1077

4216

R

4

Int64

Wh

T2 Total active energy

0x107C

4221

0x107B

4220

R

4

Int64

VARh

T1 Forward reactive energy

0x1080

4225

0x107F

4224

R

4

Int64

VARh

T2 Forward reactive energy

0x1084

4229

0x1083

4228

R

4

Int64

VARh

T1 Reverse reactive energy

0x1088

4233

0x1087

4232

R

4

Int64

VARh

T2 Reverse reactive energy

0x108C

4237

0x108B

4236

R

4

Int64

VARh

T1 Total reactive energy

0x1090

4241

0x108F

4240

R

4

Int64

VARh

T2 Total reactive energy

Energy values - 32-bit floating point

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

Total energy (cannot be rest)

0xB02C

45101

0xB02B

45100

R

2

Float32

Wh

Forward active energy

0xB02E

45103

0xB02D

45102

R

2

Float32

Wh

Reverse active energy

0xB030

45105

0xB02F

45104

R

2

Float32

VARh

Forward reactive energy

0xB032

45107

0xB031

45106

R

2

Float32

VARh

Reverse reactive energy

0xB038

45113

0xB037

45112

R

2

Float32

Wh

Total active energy

0xB03A

45115

0xB039

45114

R

2

Float32

VARh

Total reactive energy

Partial energy

0xB034

45109

0xB033

45108

R

2

Float32

Wh

Forward partial active energy

Energy by tariff

0xB040

45121

0xB03F

45120

R

2

Float32

Wh

T1 Forward active energy

0xB042

45123

0xB041

45122

R

2

Float32

Wh

T2 Forward active energy

0xB044

45125

0xB043

45124

R

2

Float32

Wh

T1 Reverse active energy

0xB046

45127

0xB045

45126

R

2

Float32

Wh

T2 Reverse active energy

0xB048

45129

0xB047

45128

R

2

Float32

Wh

T1 Total active energy

0xB04A

45131

0xB049

45130

R

2

Float32

Wh

T2 Total active energy

0xB04C

45133

0xB04B

45132

R

2

Float32

VARh

T1 Forward reactive energy

0xB04E

45135

0xB04D

45134

R

2

Float32

VARh

T2 Forward reactive energy

0xB050

45137

0xB04F

45136

R

2

Float32

VARh

T1 Reverse reactive energy

0xB052

45139

0xB051

45138

R

2

Float32

VARh

T2 Reverse reactive energy

0xB054

45141

0xB053

45140

R

2

Float32

VARh

T1 Total reactive energy

0xB056

45143

0xB055

45142

R

2

Float32

VARh

T2 Total reactive energy

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?