7EN02-0468-01

Manufacturer-specific VIFE codes

The manufacturer-specific VIFE codes in the table below are used by the meter when the VIF equals FF hex (1111 1111 bin).

NOTE: E denotes the extension bit; the hex value assumes E = 0.

Description

bin

hex

Export energy value

E000 1001

09

Partial energy value

E000 1101

0D

Current

E000 0000

00

Voltage L-N

E000 0100

04

Power Factor

E000 1010

0A

Frequency

E000 1011

0B

Active tariff

E001 0000

10

Tariff control mode

E001 0001

11

Number of phases

E010 0001

21

Number of wires

E010 0010

22

Power system configuration

E010 0011

23

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?