7EN02-0468-01

Setting up combination code

The meter allows you to display the total energy (usage) based on the combination code. The combination code is in accordance with different calculation methods as shown below:

Code

Total (active) energy

C-01

Forward only

C-04

Reverse only

C-05

Forward + Reverse

C-06

Reverse - Forward

C-09

Forward - Reverse

C-10

Forward - Reverse

To change the combination code, follow these steps:

  1. Scroll with the buttons to Program mode 3 (Pro-3).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Enter the 4 digit password (default: 0000): scroll with the buttons and select each digit 0 – 9, hold the up-arrow button for 3 seconds to confirm each digit.
  4. Scroll to combination code (C-xx) page.
  5. Hold the up-arrow button for 5 seconds to enter program mode.
  6. When the value starts blinking: select 01 / 04 / 05 / 06 / 09 / 10.
  7. Hold both buttons for 3 seconds to confirm the new setting.
  8. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?