7EN02-0468-01

Meter screen menus

The meter screens are grouped logically, according to their function. The meter’s display screen and the buttons allow you to view the various parameters.

You can access any available meter screen by first selecting the main menu (top level) screen that contains it.

NOTE: The menu screens shown throughout this user manual depicts when tariff mode is selected for T1 unless otherwise specified.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?