7EN02-0468-01

Feature summary

Function

iEM2435

iEM2455

4 quadrant energy measurements, partial and total energy counter

Total of forward and reverse active energy

Total of forward and reverse reactive energy

Power:

  • Active power (kW)

  • Apparent power (kVA)

  • Reactive power (kVAR)

Voltage, current, frequency and power factor

2 tariff control through command register

Pulse outputs

Communication

M-Bus

RS-485 Modbus

MID / MIR compliant

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?