Meter setup and status
|
RFT |
SE |
Action |
Size |
Type |
Units |
Description |
||
|---|---|---|---|---|---|---|---|---|
|
Address |
Register |
Address |
Register |
|||||
|
0x0725 |
1830 |
0x0724 |
1829 |
R |
1 |
UInt16 |
- |
Power on off counter Default: 1 |
|
0x07DE |
2015 |
0x07DD |
2014 |
R |
1 |
UInt16 |
- |
Number of phases (Always 1) |
|
0x07DF |
2016 |
0x07DE |
2015 |
R |
1 |
UInt16 |
- |
Number of wires (Always 2) |
|
0x07E0 |
2017 |
0x07DF |
2016 |
R |
1 |
UInt16 |
- |
Power system (Always 0 = 1PH2W L-N) |
|
0x07E1 |
2018 |
0x07E0 |
2017 |
R |
1 |
UInt16 |
Hz |
Nominal frequency Default: 50 |
|
0x07E4 |
2021 |
0x07E3 |
2020 |
R |
2 |
Float32 |
A |
Meter amps Default: 100 |