7EN02-0468-01

Primary VIFE codes used by the meter

The primary VIFE codes in the table below are used by the meter when the VIF equals FD hex (1111 1101 bin).

NOTE: E denotes the extension bit; x in the hex value is determined by bits 7-4 of the VIFE.

Primary VIFE codes

bin

hex

Additional information

Manufacturer

E000 1010

xA

Model

E000 1100

xC

Voltage

E100 1001

x9

Volts with a resolution of 100

Current

E101 1100

xC

Amps with a resolution of 100

Error flag

E001 0111

x7

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?