7EN02-0468-01

Setting up scrolling time

In automatic scroll, for every 10 seconds (default setting) the meter displays the next programmed data page.

To change the scrolling time, follow these steps:

  1. Scroll with the buttons to Program mode 2 (Pro-2).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Scroll to LCD cycle time (SEC) page.
  4. Hold the up-arrow button for 5 seconds to enter program mode.
  5. When the value starts blinking: select the new value between 1 – 30 seconds.
  6. Hold both buttons for 3 seconds to confirm the new scrolling time.
  7. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?