7EN02-0468-01

Energy settings

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

0x196A

6507

0x1969

6506

R/WC

1

UInt16

-

Combined Code

  • 01 (F)
  • 04 (R)
  • 05 (F+R) (default)
  • 06 (R-F)
  • 09 (F-R)
  • 10 (F-R)
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?