7EN02-0468-01

Resetting day counter

The meter is equipped with a day counter for consumed energy. The consumed energy is the energy forward calculated and can be reset to zero (0).
To reset the day counter to zero (0), follow these steps:
  1. Scroll with the buttons to resettable kWh (RSET) page in the main menu.
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. When the value starts blinking: hold the up-arrow button for 5 seconds to reset.
  4. The LCD displays OK when the day counter is reset.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?