7EN02-0468-01

Overview of meter functions

The iEM2435 / iEM2455 is a single phase meter which measures the forward and reverse energy with a blue backlight LCD display.

The key features of the meters are as follows:

  • Current, voltage, and energy measurements

  • Total of forward and reverse active energy, total of forward and reverse reactive energy, and active power measurements

  • Pulse outputs

  • Tariff measurement

  • Communication via M-Bus or RS-485 Modbus

For applications, feature details and complete specifications, see the iEM2435 / iEM2455 datasheet at www.se.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?