7EN02-0468-01

Setting up parity (only iEM2455)

The Modbus (iEM2455) parity can be set to EvEn, nonE or odd. The M-bus (iEM2435) parity is always EvEn.
To change the parity, follow these steps:
  1. Scroll with the buttons to Program mode 3 (Pro-3).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Enter the 4 digit password (default: 0000): scroll with the buttons and select each digit 0 – 9, hold the up-arrow button for 3 seconds to confirm each digit.
  4. Scroll to parity (PRTY) page.
  5. Hold the up-arrow button for 5 seconds to enter program mode.
  6. When the value starts blinking: select EvEn / nonE / odd.
  7. Hold both buttons for 3 seconds to confirm the new setting.
  8. The LCD displays OK when the setting is confirmed.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?