7EN02-0468-01

Meter description

 

A

Protection covers

 

B

Sealing points

 

C

Blue backlight LCD display

 

D

Down-arrow button (touch sensitive)

 

E

Up-arrow button (touch sensitive)

 

F

Active energy consumption LED (B=10000 imp/kWh)

 

G

Reactive energy consumption LED (A=10000 imp/kVARh)

 
NOTE: The protection covers (A) must be installed and sealed to the sealing points (B) with the steel cable of 1 mm (0.04 in) diameter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?