7EN02-0468-01

Command interface

RFT

SE

Action

Size

Type

Units

Description

Address

Register

Address

Register

0x1482

5251

0x1481

5250

W

1

UInt16

-

Requested command

0x1483

5252

0x1482

5251

W

1

UInt16

-

Reserved for future use

0x1484 - 0x148D

5253 - 5262

0x1483 - 0x148C

5252 - 5261

W

1

UInt16

-

Command parameter 001 -010

0x14FF

5376

0x14FE

5375

R/W

1

UInt16

-

Command status

0x1500

5377

0x14FF

5376

R/W

1

UInt16

-

Command result codes:

  • 0 = Valid and successful command

  • 3000 = Invalid command

  • 3001 = Invalid parameter

  • 3002 = Invalid number of parameters

  • 3007 = Command is valid but the operation was not performed

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?