7EN02-0468-01

Resetting power down counter

The power down counter registers the number of times the meter has been turned off.
To reset the power down counter, follow these steps:
  1. Scroll with the buttons to Program mode 3 (Pro-3).
  2. Hold the up-arrow button for 3 seconds to enter the menu.
  3. Enter the 4 digit password (default: 0000): scroll with the buttons and select each digit 0 – 9, hold the up-arrow button for 3 seconds to confirm each digit.
  4. Scroll to power down counter (PCNT) page.
  5. Hold the up-arrow button for 5 seconds to enter program mode.
  6. When the value starts blinking: hold both buttons for 3 seconds to reset.
  7. The LCD displays OK when the power down counter is reset.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?