7EN02-0468-01

Meter information

NOTE: E denotes the extension bit; the hex value assumes E = 0.

Data format

Primary VIF Extension

Description

bin

hex

0D

E000 1010

0A

Manufacturer

  • “Schneider Electric” in 18-byte ASCII format

0D

E000 1100

0C

Model in ASCII format

03

E0001 0111

17

Meter error codes:

  • 0 = Code 101: error in executable firmware code
  • 1 = Code 102: calibration data is missing or has errors

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?