System
|
RFT |
SE |
Action |
Size |
Type |
Units |
Description |
||
|---|---|---|---|---|---|---|---|---|
|
Address |
Register |
Address |
Register |
|||||
|
0x001E |
31 |
0x001D |
30 |
R |
20 |
UTF8 |
- |
Meter name Default: Power Meter |
|
0x0032 |
51 |
0x0031 |
50 |
R |
20 |
UTF8 |
- |
Meter model Default: iEM2455 |
|
0x0046 |
71 |
0x0045 |
70 |
R |
20 |
UTF8 |
- |
Manufacturer Default: Schneider Electric |
|
0x005A |
100 |
0x0059 |
99 |
R |
1 |
UInt16 |
- |
Meter code |
|
0x0082 |
131 |
0x0081 |
130 |
R |
2 |
UInt32 |
- |
Serial number |
|
0x0088 |
137 |
0x0087 |
136 |
R |
5 |
UTF8 |
- |
Hardware revision in x.x.x format Default: 1.0.0 NOTE: The first number is the major version, the second number is the minor
version, and the third number is normally not used.
|
|
0x0665 |
1638 |
0x0664 |
1637 |
R |
1 |
UInt16 |
- |
Present firmware version |