7EN02-0468-01

Telegram information for meter configuration

You can use the information provided in this section to write to the meter using a SND_UD function.

You can also configure the meter using the M-Bus tool available from www.se.com.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?