Primary VIF used by the meter
|
Primary VIF |
bin |
hex |
Description |
|---|---|---|---|
|
Energy |
E000 0011 |
x3 |
Wh with a resolution of 100 |
|
Power |
E000 1110 |
xE |
kW with a resolution of 103 |
|
Bus address |
E111 1010 |
xD |
Data type C (unsigned integer), as detailed in the M-Bus protocol documentation |
|
Primary VIFE |
1111 1101 |
FD |
Indicates that the first VIFE is a primary VIF extension |
|
Manufacturer-specific VIFE |
1111 1111 |
FF |
Indicates that the next VIFE is manufacturer specific |