PROFIBUS Acyclic Data
TeSys™ island supports the following slot and index ranges for PROFIBUS acyclic dataset exchange. For PROFIBUS acyclic datasets supported by TeSys island, refer to PROFINET Acyclic Data for more information. PROFIBUS and PROFINET share the same acyclic datasets for TeSys™ island.
PROFIBUS Acyclic Data
|
Dataset |
Slot |
Index |
Comment |
|---|---|---|---|
|
(Reserved) |
0 |
— |
Reserved in PROFIBUS, not mapped to any avatar or device |
| 1 |
— |
Index 0 reserved for System Control |
|
|
System Diagnostic |
1 | 1 |
— |
|
System Energy 1 |
1 | 2 |
Includes Voltage Basic and Voltage Enhanced |
|
System Energy 2 |
1 | 3 |
Includes Power Basic and Energy Basic |
|
System Asset Management |
1 | 4 |
— |
|
System Combined Output |
1 | 5 |
— |
|
System Time |
1 | 6 |
— |
|
Control |
2–22 | 0 |
— |
|
Energy |
2–22 | 1 |
— |
|
Diagnostic |
2–22 | 2 |
— |
|
Asset Management |
101–121 | 0 |
— |