8536IB1905EN-05

Pump

This function block is used to manage a pump.

Pump Function Block

Modbus TCP Inputs — Pump

Input Name Address Starting Bit Size (Bits)
Run 1 8501 0 1
Trip Reset 8501 3 1

Modbus TCP Outputs — Pump

Output Name Address Starting Bit Size (Bits)
Thermal Overload Time To Reset 450 0 16
Protection Trip Message 1 452 0 16
Protection Trip Message 2 453 0 16
Protection Alarm Message 1 461 0 16
Protection Alarm Message 2 462 0 16
IRMS Average 500 0 32
Thermal Overload Time To Trip 511 0 16
Ready 3201 0 1
Run 1 Status 3201 1 1
Tripped 3201 2 1
Alarm 3201 3 1
Load Running 3201 8 1
Ready To Reset 3201 9 1
Load Starting 3201 15 1
Asset Alarm 3202 3 1
Upstream Voltage Present 1 3202 12 1
Bypass Command Status 3215 0 1
Local Forward Status 3215 1 1
PV Control Input 0 Status 3215 5 1
PV Control Input 1 Status 3215 6 1
Manual Mode Override Status 3215 7 1
Predictive Alarm Status 3217 0 16
PV Input 0 3224 0 16
PV Input 1 3225 0 16
PV Input 2 3226 0 16
PV Input 3 3227 0 16
PV Input 4 3228 0 16
PV Switch 0 3230 0 1
PV Switch 1 3230 1 1
PV Switch 2 3230 2 1
PV Switch 3 3230 3 1
PV Switch 4 3230 4 1
Motor Thermal Capacity Used 9630 0 8
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?