Asset Management
This function block returns maintenance and product identification information of the devices.
Modbus TCP Outputs—Asset Management
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Number of Device Power Cycles |
24 |
0 |
32 |
|
Number of Contactor Cycles |
26 |
0 |
32 |
|
Time (module) On |
28 |
0 |
32 |
|
Time Switch On |
30 |
0 |
32 |
|
Lifetime Average IRMS |
35 |
0 |
32 |
|
Maximum IRMS |
32 |
0 |
16 |
|
Number of Device Events |
33 |
0 |
16 |
|
Average Lifetime Voltage |
34 |
0 |
16 |
|
Number of SIL* Starter Stops |
40 |
0 |
32 |
|
Maximum Average Voltage |
32 |
0 |
16 |