Energy
Avatar Power Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Unit |
Minimum |
Maximum |
Step |
Description |
|---|---|---|---|---|---|---|---|---|
|
Instantaneous Total Active Power |
DINT |
32 |
0.001 |
kW |
-2,147,483,648 |
2,147,483,647 |
1 |
Returns the total Active Power for the avatar. |
|
Maximum Total Active Power |
DINT |
32 |
0.001 |
kW |
-9,999,999 |
9,999,999 |
1 |
Returns the maximum value of total active power for the avatar. |
|
Maximum Total Active Power Timestamp |
DT |
64 |
— |
Date, Time |
— |
— |
— |
Provide date and time when maximum total active Power value has been recorded. |
|
Instantaneous Total Reactive Power |
DINT |
32 |
0.001 |
kVAR |
-9,999,999 |
9,999,999 |
1 |
Returns the total Reactive Power value for the avatar. |
|
Maximum Total Reactive Power |
DINT |
32 |
0.001 |
kVAR |
-9,999,999 |
9,999,999 |
1 |
Returns the maximum value of Reactive Power for the avatar. |
|
Maximum Total Reactive Power Timestamp |
DT |
64 |
— |
Date, Time |
— |
— |
— |
Provide date and time when total maximum total Reactive Power value has been recorded |
|
True Power Factor |
USINT |
8 |
0.01 |
— |
0 |
100 |
1 |
Returns the true Power factor value. |
|
Minimum True Power Factor |
USINT |
8 |
0.01 |
— |
0 |
100 |
1 |
Returns the true Power factor minimum value. |
|
Maximum True Power Factor |
USINT |
8 |
0.01 |
— |
0 |
100 |
1 |
Returns the true Power factor maximum value. |
|
Minimum True Power Factor Timestamp |
DT |
64 |
— |
Date, Time |
— |
— |
— |
Provide date and time when Minimum Power Factor value has been recorded. |
|
Maximum True Power Factor Timestamp |
DT |
64 |
— |
Date, Time |
— |
— |
— |
Provide date and time when Maximum Power Factor value has been recorded. |
Avatar Energy Inputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Unit |
Minimum |
Maximum |
Step |
Description |
|---|---|---|---|---|---|---|---|---|
|
Set Total Active Energy |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Command to set the Total Active Energy value to Total Active Energy Preset value. 0 = no, 1 = yes |
|
Set Total Reactive Energy |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Command to set the Total Reactive Energy value to Total Reactive Energy Preset value. 0 = no, 1 = yes |
|
Total Active Energy Preset Value |
UDINT |
32 |
0.001 |
kWh |
0 |
4,294,967,295 |
1 |
Preset the Total Active Energy value. |
|
Total Reactive Energy Preset Value |
UDINT |
32 |
0.001 |
kVARh |
0 |
4,294,967,295 |
1 |
Preset the Total Reactive Energy value. |
|
Run Record ToU Channel 1 |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Record Time of Use Channel 1 start command. |
|
Run Record ToU Channel 2 |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Record Time of Use Channel 2 start command. |
|
Run Record ToU Channel 3 |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Record Time of Use Channel 3 start command. |
|
Run Record ToU Channel 4 |
BOOL |
1 |
1 |
— |
0 |
1 |
1 |
Record Time of Use Channel 4 start command. |
Avatar Energy Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Unit |
Minimum |
Maximum |
Step |
Description |
|---|---|---|---|---|---|---|---|---|
|
Total Active Energy |
UDINT |
32 |
0.001 |
kWh |
0 |
4,294,967,295 |
1 |
Returns the Total Active Energy value. |
|
Total Reactive Energy |
UDINT |
32 |
0.001 |
kVARh |
0 |
999,999,999 |
1 |
Returns the Total Reactive Energy value |
|
ToU Total Active Energy Channel 1 |
UDINT |
32 |
0.001 |
kWh |
0 |
999,999,999 |
1 |
Returns the Total Active Energy Value that has been accumulated while the Channel is enabled/active. |
|
ToU Total Active Energy Channel 2 |
UDINT |
32 |
0.001 |
kWh |
0 |
999,999,999 |
1 |
|
|
ToU Total Active Energy Channel 3 |
UDINT |
32 |
0.001 |
kWh |
0 |
999,999,999 |
1 |
|
|
ToU Total Active Energy Channel 4 |
UDINT |
32 |
0.001 |
kWh |
0 |
999,999,999 |
1 |
|
|
ToU Total Reactive Energy Channel 1 |
UDINT |
32 |
0.001 |
kVARh |
0 |
999,999,999 |
1 |
Returns the Total Reactive Energy Value that has been accumulated while the Channel is enabled/active. |
|
ToU Total Reactive Energy Channel 2 |
UDINT |
32 |
0.001 |
kVARh |
0 |
999,999,999 |
1 |
|
|
ToU Total Reactive Energy Channel 3 |
UDINT |
32 |
0.001 |
kVARh |
0 |
4,294,967,295 |
1 |
|
|
ToU Total Reactive Energy Channel 4 |
UDINT |
32 |
0.001 |
kVARh |
0 |
4,294,967,295 |
1 |