Power Supply
This function block is used to manage a power supply.
Modbus TCP Inputs—Power Supply
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Run 1 |
8501 |
0 |
1 |
|
Trip Reset |
8501 |
3 |
1 |
Modbus TCP Outputs—Power Supply
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Protection Trip Message 1 |
452 |
0 |
16 |
|
Protection Trip Message 2 |
453 |
0 |
16 |
|
Protection Alarm Message 1 |
461 |
0 |
16 |
|
Protection Alarm Message 2 |
462 |
0 |
16 |
|
IRMS Average |
500 |
0 |
32 |
|
Ready |
3201 |
0 |
1 |
|
Run 1 Status |
3201 |
1 |
1 |
|
Tripped |
3201 |
2 |
1 |
|
Alarm |
3201 |
3 |
1 |
|
Load Running |
3201 |
8 |
1 |
|
Ready to Reset |
3201 |
9 |
1 |
|
Load Starting |
3201 |
15 |
1 |
|
Asset Alarm |
3202 |
3 |
1 |
|
Upstream Voltage Present 1 |
3202 |
12 |
1 |