8536IB1905EN-05

TeSys island Modbus TCP Function Block Data

This section contains generic function block diagrams and register data that can be used to assist with PLC programming. For the I/O data and value ranges available at the system and avatar level, refer to Data Descriptions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?