Asset Management
System Product Data Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Unit |
Min. |
Max. |
Step |
Description |
|
|---|---|---|---|---|---|---|---|---|---|
|
Base MAC Address |
DT_MAC |
48 |
— |
— |
— |
— |
— |
MAC address of Fieldbus Ethernet port 1. |
|
System Maintenance Data Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Unit |
Min. |
Max. |
Step |
Description |
|
|---|---|---|---|---|---|---|---|---|---|
|
Time (module) ON |
UDINT |
32 |
1 |
Hour |
0 |
4,294,967,295 |
1 |
This register indicates the time that the module has been powered on in its lifetime. |
|
|
Number of Events (Device Events) |
UINT |
16 |
1 |
— |
0 |
65,535 |
1 |
This register attempts to indicate number of times this module has experienced a device event. This value does not include device event which prevent the saving or corruption of the NVM. |
|