8536IB1905EN-05

TeSys island I/O Data

TeSys™ island generates and sends advanced data to the PLC to enhance machine efficiency and improve asset management. I/O data is available at the system and the avatar level. Types of I/O data include control, diagnostics, energy, and asset management. The following tables describe the inputs and outputs available for the avatars. The following tables can be used to assist in third party PLC function block programming when pre-defined function blocks are not available.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?