8536IB1905EN-05

Understanding Avatar Command and Status Bits

The EDS file contains details about the data for the various avatar commands and statuses. These are described as A1_Commands (Avatar 1 commands), A2_Commands1 (first set of Avatar 2 commands), A2_Commands2 (last set of Avatar 2 commands), etc.

In many programming tools, the parameters are only described as full bytes. However, the EDS file contains the detailed descriptions of each bit. To access the information if your programming tool does not display it, open the EDS file with an EDS file viewer such as EZ-EDS. If you select the parameter (such as A2_Commands1 shown below) and then select Enumerate, a full description of each bit displays.

EZ-EDS Enumerate

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?