8536IB1905EN-05

Precautions

Read and understand the following precautions before performing any procedures in this guide.

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • This equipment must only be installed and serviced by qualified electrical personnel.
  • Turn off all power supplying this equipment before working on or inside this equipment.
  • Use only the specified voltage when operating this equipment and any associated products.
  • Always use a properly rated voltage sensing device to confirm power is off.
  • Use appropriate interlocks where personnel and/or equipment hazards exist.
  • Power line circuits must be wired and protected in compliance with local and national regulatory requirements.
  • Apply appropriate personal protective equipment (PPE) and follow safe electrical work practices per NFPA 70E, NOM-029-STPS, or CSA Z462 or local equivalent.
Failure to follow these instructions will result in death or serious injury.
WARNING
Unintended equipment operation
  • Do not disassemble, repair, or modify this equipment. There are no user serviceable parts.
  • Install and operate this equipment in an enclosure appropriately rated for its intended application environment.
  • Each implementation of this equipment must be individually and thoroughly tested for proper operation before being placed into service.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

WARNING: This product can expose you to chemicals including Antimony oxide (Antimony trioxide), which is known to the State of California to cause cancer. For more information go to www.P65Warnings.ca.gov .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?