Motor Two Speeds Two Directions – SIL Stop, W. Cat 1/2 Dataset
Motor Two Speeds Two Directions SIL Stop W. Cat 1/2 * Dataset Input Data
|
Byte 0 |
Reset Max IRMS |
Reset Trip Counter |
Reset Alarm Counter |
Trip Reset |
ON/OFF High Speed Reverse |
ON/OFF Low Speed Reverse |
ON/OFF High Speed Forward |
ON/OFF Low Speed Forward |
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 1 |
— |
— |
— |
— |
Run TOU Channel 4 |
Run TOU Channel 3 |
Run TOU Channel 2 |
Run TOU Channel 1 |
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
Motor Two Speeds Two Directions SILStop W. Cat 1/2 Dataset Output Data
|
Byte 0 |
High Speed Forward Status |
Asset Alarm |
— |
Upstream Voltage Present (Device 1) |
Alarm |
Tripped |
Low Speed Forward Status |
Ready |
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 1 |
Load Starting |
High Speed Reverse Status |
Low Speed Reverse Status |
Upstream Voltage Present (Device 4) |
Upstream Voltage Present (Device 3) |
Upstream Voltage Present (Device 2) |
Ready to Reset |
Load Operating |
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 2 |
Irms Average [MSB] |
|||||||
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 3 |
Irms Average |
|||||||
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 4 |
Irms Average |
|||||||
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|
|
Byte 5 |
Irms Average [LSB] |
|||||||
|
7 |
6 |
5 |
4 |
3 |
2 |
1 |
0 |
|