Power Interface Module without I/O (Measure)
This function block is used to monitor current on an external power device, such as a solid-state relay, soft starter, or variable speed drive.
Modbus TCP Inputs—PIM without I/O (Measure)
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Trip Reset |
8501 |
3 |
1 |
Modbus TCP Outputs—PIM without I/O (Measure)
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Thermal Overload Time to Reset |
450 |
0 |
16 |
|
Protection Trip Message 1 |
452 |
0 |
16 |
|
Protection Trip Message 2 |
453 |
0 |
16 |
|
Protection Alarm Message 1 |
461 |
0 |
16 |
|
Protection Alarm Message 2 |
462 |
0 |
16 |
|
Motor Temperature |
464 |
0 |
16 |
|
IRMS Average |
500 |
0 |
32 |
|
Thermal Overload Time to Trip |
511 |
0 |
16 |
|
Ready |
3201 |
0 |
1 |
|
Tripped |
3201 |
2 |
1 |
|
Alarm |
3201 |
3 |
1 |
|
Load Running |
3201 |
8 |
1 |
|
Ready to Reset |
3201 |
9 |
1 |
|
Load Starting |
3201 |
15 |
1 |
|
Upstream Voltage Present 1 |
3202 |
12 |
1 |
|
Motor Thermal Capacity Used |
9630 |
0 |
8 |