Asset Management
Avatar Maintenance Data Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Value |
Description |
|
|---|---|---|---|---|---|---|
|
Time (module) On |
UDINT |
32 |
1 |
0 to 4,294,967,295 |
Indicates the time that the module has been powered on in its lifetime (in hours). |
|
|
Time Switch On |
UDINT |
32 |
1 |
0 to 4,294,967,295 |
Indicates the time (in hours) that the contactor has been in the closed state. |
|
|
Number of Events (Device Events) |
UINT |
16 |
1 |
0 to 65,535 |
Indicates the number of times this module has experienced a device event. This value does not include device events which corrupt or prevent the saving of the non-volatile memory. |
|
|
Number of Contactor Cycles |
UDINT |
32 |
1 |
0 to 4,294,967,295 |
Indicates number of times the contactor has been commanded to the closed state from the open state. |
|
|
Number of Device Power Cycles |
UDINT |
32 |
1 |
0 to 4,294,967,295 |
Indicates number of times the device has been powered on. |
|
|
Number of SIL Starter Stops* |
UDINT |
32 |
1 |
0 to 4,294,967,295 |
Indicates the number of mirror relay operations. |
|
|
Max. IRMS |
UINT |
16 |
0.1 |
0 to 65,535 |
Indicates maximum current (A) the device has measured in its lifetime. |
|
|
Lifetime Average IRMS |
UDINT |
32 |
0.001 |
0 to 4,294,967,295 |
Lifetime average current (A) measured by the device (Total Current / Time Current ON). |
|
|
Max. Average Voltage |
UINT |
16 |
1 |
0 to 65,535 |
Indicates maximum voltage (V) the device has measured in its lifetime. |
|
|
Average Lifetime Voltage |
UNIT |
16 |
1 |
0 to 65,535 |
Indicates average lifetime voltage (V) measured. |
|