8536IB1905EN-05

System Time

This function block returns the date and time of the system device.

System Time Function Block

Modbus TCP Outputs — System Time

Output Name Address Starting Bit Size (Bit)

System Time

2100

0

64

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?