Motor Two Speeds Two Directions - SIL Stop, W. Cat 1/2
This function block is used to manage a two speed motor in two directions (forward and reverse) with Stop Category 0 or Stop Category 1 function compliance for Wiring Category 1 and Category 2.*
Modbus TCP Inputs
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Run Forward High |
8501 |
0 |
1 |
|
Run Reverse High |
8501 |
1 |
1 |
|
Trip Reset |
8501 |
3 |
1 |
|
Run Forward Low |
8501 |
6 |
1 |
|
Run Reverse Low |
8501 |
7 |
1 |
Modbus TCP Outputs
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Thermal Overload Time to Reset |
450 |
0 |
16 |
|
Protection Trip Message 1 |
452 |
0 |
16 |
|
Protection Trip Message 2 |
453 |
0 |
16 |
|
Protection Alarm Message 1 |
461 |
0 |
16 |
|
Protection Alarm Message 2 |
462 |
0 |
16 |
|
IRMS Average |
500 |
0 |
32 |
|
Thermal Overload Time to Trip |
511 |
0 |
16 |
|
Ready |
3201 |
0 |
1 |
|
Tripped |
3201 |
2 |
1 |
|
Alarm |
3201 |
3 |
1 |
|
Run Forward Low Status |
3201 |
5 |
1 |
|
Run Forward High Status |
3201 |
6 |
1 |
|
Load Running |
3201 |
8 |
1 |
|
Ready to Reset |
3201 |
9 |
1 |
|
Run Reverse Low Status |
3201 |
12 |
1 |
|
Run Reverse High Status |
3201 |
13 |
1 |
|
Load Starting |
3201 |
15 |
1 |
|
Asset Alarm |
3202 |
3 |
1 |
|
Upstream Voltage Present 1 |
3202 |
12 |
1 |
|
Upstream Voltage Present 2 |
3202 |
13 |
1 |
|
Upstream Voltage Present 3 |
3202 |
14 |
1 |
|
Upstream Voltage Present 4 |
3202 |
15 |
1 |
|
Motor Thermal Capacity Used |
9630 |
0 |
8 |