8536IB1905EN-05

PROFIBUS Cyclic Data

When importing the General Station Description (GSD) or General Station Description Markup Language (GSDML) file into your programming environment and inserting each avatar into the appropriate slots, the information is displayed with input and output bytes.

The PROFIBUS cyclic data is structured similar to the PROFINET cyclic data and therefore, share the same input and output data for the avatars listed in the tables in PROFINET Cyclic Data.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?