Digital I/O
This function block provides information about the Digital I/O avatar. The Digital I/O avatar has four inputs and two outputs.
Modbus TCP Inputs—Digital I/O
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Digital Output 1 |
8501 |
8 |
1 |
|
Digital Output 2 |
8501 |
9 |
1 |
Modbus TCP Outputs—Digital I/O
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Digital Input 0 Status |
3201 |
4 |
1 |
|
Digital Input 1 Status |
3201 |
5 |
1 |
|
Digital Input 2 Status |
3201 |
6 |
1 |
|
Digital Input 3 Status |
3201 |
7 |
1 |