Control
Avatar Control Inputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Value |
Description |
|
|---|---|---|---|---|---|---|
|
Trip Reset |
BOOL |
1 |
1 |
0, 1 |
Command
to reset an avatar trip event |
|
|
Run 1 |
BOOL |
1 |
1 |
0, 1 |
Command
to Avatar Forward Switch. |
|
|
Run 2 |
BOOL |
1 |
1 |
0, 1 |
Command to Avatar Forward redundant
Switch for Wiring Category 3 and Wiring Category 4 avatars. |
|
|
Run Forward |
BOOL |
1 |
1 |
0, 1 |
Command
to Avatar Forward Switch. |
|
|
Run Reverse |
BOOL |
1 |
1 |
0, 1 |
Command
to close the Reverse switch with Reverser Avatar |
|
|
Run Forward Low |
BOOL |
1 |
1 |
0, 1 |
Command
to start Motor forward with Low Speed |
|
|
Run Forward High |
BOOL |
1 |
1 |
0, 1 |
Command
to start Motor forward with High Speed |
|
|
Run Reverse Low |
BOOL |
1 |
1 |
0, 1 |
Run Reverse
Low Speed command |
|
|
Run Reverse High |
BOOL |
1 |
1 |
0, 1 |
Run Reverse
High Speed command |
|
|
Logic Output 1 |
BOOL |
1 |
1 |
0, 1 |
Command
to Close Logical output 1 |
|
|
Logic Output 2 |
BOOL |
1 |
1 |
0, 1 |
Command
to Close Logical output 2 |
|
|
Digital Output 0 |
BOOL |
1 |
1 |
0, 1 |
Command
to close Digital output 0 |
|
|
Digital Output 1 |
BOOL |
1 |
1 |
0, 1 |
Command
to close Digital output 1 |
|
|
Analog Output 0 |
INT |
16 |
1 |
–32,768 to 32,767 |
Value to be written to Analog output 0 |
|
Avatar Control Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Value |
Description |
|
|---|---|---|---|---|---|---|
|
Ready |
BOOL |
1 |
1 |
0, 1 |
The avatar
is ready to be controlled (all Devices in the avatar are Ready). |
|
|
Upstream Voltage Present 1 |
BOOL |
1 |
1 |
0, 1 |
The avatar
has detected that Upstream main power of its first Device is present
(Breaker closed). |
|
|
Upstream Voltage Present 2 |
BOOL |
1 |
1 |
0, 1 |
The avatar
has detected that Upstream main power of its second Device (if available)
is present. |
|
|
Upstream Voltage Present 3 |
BOOL |
1 |
1 |
0, 1 |
The avatar
has detected that Upstream main power of its third Device (if available)
is present. |
|
|
Upstream Voltage Present 4 |
BOOL |
1 |
1 |
0, 1 |
The avatar
has detected that Upstream main power of its fourth Device (if available)
is present. |
|
|
Run 1 Status |
BOOL |
1 |
1 |
0, 1 |
Status of
the primary switch for Wiring Category 3 and Category 4. |
|
|
Run 2 Status |
BOOL |
1 |
1 |
0, 1 |
Status of the primary switch for Wiring
Category 3 and Category 4. |
|
|
Run Forward Status |
BOOL |
1 |
1 |
0, 1 |
Avatar Forward
Switch Feedback, |
|
|
Run Reverse Status |
BOOL |
1 |
1 |
0, 1 |
Avatar Reverse
Switch Feedback, |
|
|
Run Y Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the Y switch for Y/D avatars. |
|
|
Run D Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the D Switch for Y/D avatars. |
|
|
Run Forward Low Status |
BOOL |
1 |
1 |
0, 1 |
Motor is
running in Speed1 |
|
|
Run Forward High Status |
BOOL |
1 |
1 |
0, 1 |
Motor is
running in Speed2 |
|
|
Run Reverse Low Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the Low Speed Reverser switch. |
|
|
Run Reverse High Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the High Speed Reverser switch. |
|
|
Logic Output 1 Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the Output 1. |
|
|
Logic Output 2 Status |
BOOL |
1 |
1 |
0, 1 |
Position
of the Output 2. |
|
|
Logic Input 1 Status |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 1 of the avatar. |
|
|
Logic Input 2 Status |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 1 of the avatar. |
|
|
Digital Input Status 0 |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 0 of DIOM Avatar |
|
|
Digital Input Status 1 |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 1 of DIOM Avatar |
|
|
Digital Input Status 2 |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 2 of DIOM Avatar |
|
|
Digital Input Status 3 |
BOOL |
1 |
1 |
0, 1 |
State of
Digital Input 3 of DIOM Avatar |
|
|
Bypass Command Status |
BOOL |
1 |
1 |
0, 1 |
State of avatar if the bypass command
has been issued to continue operation and not stop due to a trip. |
|
|
Local Forward Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Local Forward Switch Feedback, |
|
|
Local Reverse Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Reverse Forward Switch Feedback, |
|
|
Local Forward Low Speed Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Local Forward Low Speed Switch Feedback, |
|
|
Local Forward High Speed Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Local Forward High Speed Switch Feedback, |
|
|
Local Reverse Low Speed Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Local Reverse Low Speed Switch Feedback, |
|
|
Local Reverse High Speed Status |
BOOL |
1 |
1 |
0, 1 |
The avatar logic is controlled by commands received on digital inputs and PLC commands are ignored during local mode. Avatar Local Reverse High Speed Switch Feedback, |
|
|
Manual Mode Override Status |
BOOL |
1 |
1 |
0, 1 |
The avatar is controlled by local
command and PV control when in manual mode. |
|
|
PV Control Input 0 Status |
BOOL |
1 |
1 |
0, 1 |
Status of PV Control Input 0 (command
to avatar after input processing). |
|
|
PV Control Input 1 Status |
BOOL |
1 |
1 |
0, 1 |
Status of PV Control Input 1 (command
to avatar after input processing). |
|
|
PV Input 0 |
INT |
16 |
1 |
–32,
768 to 32,767 |
Returns the measured value of the PV input. |
|
|
PV Input 1 |
INT |
16 |
1 |
–32,
768 to 32,767 |
||
|
PV Input 2 |
INT |
16 |
1 |
–32,
768 to 32,767 |
||
|
PV Input 3 |
INT |
16 |
1 |
–32,
768 to 32,767 |
||
|
PV Input 4 |
INT |
16 |
1 |
–32,
768 to 32,767 |
||
|
PV Switch 0 |
BOOL |
1 |
1 |
0,1 |
Positive Logic – A PV Switch input ON or a PV Input above the PV Control Level represents an ON command. Negative Logic – A PV Switch input OFF or a PV Input below the PV Control Level represents an ON command. 0 = Off, 1 = On |
|
|
PV Switch 1 |
BOOL |
1 |
1 |
1,0 |
||
|
PV Switch 2 |
BOOL |
1 |
1 |
1,0 |
||
|
PV Switch 3 |
BOOL |
1 |
1 |
1,0 |
||
|
PV Switch 4 |
BOOL |
1 |
1 |
1,0 |
||
|
Predictive Alarm Status |
UINT |
16 |
1 |
1,0 |
Predictive Alarms are triggered by combinations of protection functions alarms and PV Input conditions. The avatars support up to 10 Predictive Alarms. |
|
|
Analog Input 0 |
INT |
16 |
1 |
–32,768 to 32,767 |
Value read from the Analog input 0 |
|
|
Analog Input 1 |
INT |
16 |
1 |
–32,768 to 32,767 |
Value read from the Analog input 1 |
|
|
Load Starting |
BOOL |
1 |
1 |
0, 1 |
Returns
1 if the load is in start phase. |
|
|
Load Running |
BOOL |
1 |
1 |
0, 1 |
Set to 1
when a Run or Close command has been executed and current is flowing
in the poles (equivalent to Motor Running but also for non-motor avatars). |
|
|
Motor Temperature |
INT |
16 |
1 |
–200 to 850 |
Returns the motor temperature in °C. Depending on the Temperature Sensor type, the range is:
|
|
|
IRMS Average |
UDINT |
32 |
0.001 |
0–4,294,967,295 |
Calculate the average of the most recent phase current RMS values (A). |
|
|
Alarm |
BOOL |
1 |
1 |
0, 1 |
Avatar has
detected a protection alarm event. |
|
|
Tripped |
BOOL |
1 |
1 |
0, 1 |
Avatar has
detected a trip event. |
|
|
Ready to Reset |
BOOL |
1 |
1 |
0, 1 |
0 = Off, 1 = On |
|
|
Asset Alarm |
BOOL |
1 |
1 |
0, 1 |
Triggered
when a Power Device or SIM references within the avatar has reached
or exceeded 90% of expected durability (per Avatar Parameter). |
|
|
Motor Thermal Capacity Used |
USINT |
8 |
1 |
0–255 |
Returns the percentage (%) of the motor’s thermal capacity which has been used. |
|
|
Protection Alarm Message 1 |
UINT |
16 |
— |
0 to max. 0xFFFF |
1st Modbus register protection alarm bits: Bit 2: Ground Current Alarm Bit 3: Thermal Overload Alarm Bit 5: Jam Alarm Bit 6: Current Phase Unbalance Alarm Bit 7: Undercurrent Alarm |
|
|
Protection Alarm Message 2 |
UINT |
16 |
— |
0 to max. 0xFFFF |
2nd Modbus register protection alarm bits: Bit 3: Overcurrent Alarm Bit 6: Motor Overheat Alarm |
|
|
Protection Trip Message 1 |
UINT |
16 |
— |
0 to max. 0xFFFF |
1st Modbus register protection trip bits: Bit 2: Ground Current Trip Bit 3: Thermal Overload Trip Bit 4: Long Start Trip Bit 5: Jam Trip Bit 6: Current Phase Unbalance Trip Bit 7: Undercurrent Trip Bit 8: Stall Trip |
|
|
Protection Trip Message 2 |
UINT |
16 |
— |
0 to max. 0xFFFF |
2nd Modbus register protection trip bits: Bit 2: Phase Configuration Trip Bit 3: Overcurrent Trip Bit 4: Current Phase Loss Trip Bit 5: Current Phase Reversal Trip Bit 6: Motor Overheat Trip |
|
|
Thermal Overload Time To Trip |
UINT |
16 |
1 |
0–65535 |
Estimated time (in seconds) before a Thermal Overload trip. |
|
|
Thermal Overload Time To Reset |
UINT |
16 |
1 |
0–65535 |
Estimated time (in seconds) to wait before a reset could acknowledge a Thermal Overload trip. |
|