8536IB1905EN-05

Data Refresh Rates

When choosing the frequency of your fieldbus protocol (such as RPI or repetition rate) or the frequency of updating acyclic data in your PLC program, it is important to understand the frequency of the data updates on the island itself.

For instance, Active Energy data is updated every 100 ms. So it is not useful for the PLC program to update this acyclic data every 10 ms. However, all outputs (starters, digital outputs, analog outputs, trip resets, and other resets or presets) are updated at a frequency of <10 ms. Inputs are updated at various frequencies depending on their importance.

See the table below for more information.

Data Refresh Rates

Data Maximum update interval

Input and output status of power devices, digital I/O modules, and SIL* interface modules

for example, Run commands, contactor status (RunFwd, Tripped), digital input (DI0, DI1…)

10 ms

Analog measurements of power devices, analog I/O modules, and voltage interface modules

for example, phase current (AvgIRMS, PhaseXIRMS), phase voltage (VRMSPhaseX, AvgVRMS), power (InstActivePower, InstReactivePower, PowerFactor), energy (ActiveEnergy, ReactiveEnergy), analog inputs (MotorTemperature, AI0, AI1)

100 ms

Other data

for example, asset data: ContactorCycleCntr, TimeModuleOn, AvgIRMS (lifetime)

10 ms
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?