EtherNet/IP Acyclic Data
The TeSys™ island supports the following EtherNet/IP objects for Explicit Messaging:
EtherNet/IP Acyclic Data
| Object Name | Object Class ID | Instance | Comment |
|
System Diagnostic |
0x67 |
1 |
System is always 1. |
|
System Energy |
0x68 |
1 |
|
|
System Asset Management |
0x69 |
1 |
|
|
System Time |
0x70 |
1 |
|
|
Control |
0x6A |
10-99 |
Each avatar includes its own Control, Energy, and Diagnostic object. |
|
Energy |
0x6B |
10-99 |
|
|
Diagnostic |
0x6C |
10-99 |
|
|
Asset Management |
0x6D |
101-199 |
There is an instance of the Asset Management Object for each device. |
|
System Combined Output |
0x6F |
1 |
— |