Motor Y/D Two Directions
This function block is used to manage a wye-delta (star-delta) motor in two directions (forward and reverse).
Modbus TCP Inputs—Motor Y/D Two Directions
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Run Forward |
8501 |
0 |
1 |
|
Run Reverse |
8501 |
1 |
1 |
|
Trip Reset |
8501 |
3 |
1 |
Modbus TCP Outputs—Motor Y/D Two Directions
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Thermal Overload Time to Reset |
450 |
0 |
16 |
|
Protection Trip Message 1 |
452 |
0 |
16 |
|
Protection Trip Message 2 |
453 |
0 |
16 |
|
Protection Alarm Message 1 |
461 |
0 |
16 |
|
Protection Alarm Message 2 |
462 |
0 |
16 |
|
IRMS Average |
500 |
0 |
32 |
|
Thermal Overload Time to Trip |
511 |
0 |
16 |
|
Ready |
3201 |
0 |
1 |
|
Run Forward Status |
3201 |
1 |
1 |
|
Tripped |
3201 |
2 |
1 |
|
Alarm |
3201 |
3 |
1 |
|
Run Y Status |
3201 |
6 |
1 |
|
Run D Status |
3201 |
7 |
1 |
|
Load Running |
3201 |
8 |
1 |
|
Ready to Reset |
3201 |
9 |
1 |
|
Load Starting |
3201 |
15 |
1 |
|
Run Reverse Status |
3202 |
1 |
1 |
|
Asset Alarm |
3202 |
3 |
1 |
|
Upstream Voltage Present 1 |
3202 |
12 |
1 |
|
Upstream Voltage Present 2 |
3202 |
13 |
1 |
|
Upstream Voltage Present 3 |
3202 |
14 |
1 |
|
Upstream Voltage Present 4 |
3202 |
15 |
1 |
|
Bypass Command Status |
3215 |
0 |
1 |
|
Local Forward Status |
3215 |
1 |
1 |
|
Manual Mode Override Status |
3215 |
7 |
1 |
|
Local Reverse Status |
3216 |
1 |
1 |
|
Predictive Alarm Status |
3217 |
0 |
16 |
|
PV Input 0 |
3224 |
0 |
16 |
|
PV Input 1 |
3225 |
0 |
16 |
|
PV Input 2 |
3226 |
0 |
16 |
|
PV Input 3 |
3227 |
0 |
16 |
|
PV Input 4 |
3228 |
0 |
16 |
|
PV Switch 0 |
3230 |
0 |
1 |
|
PV Switch 1 |
3230 |
1 |
1 |
|
PV Switch 2 |
3230 |
2 |
1 |
|
PV Switch 3 |
3230 |
3 |
1 |
|
PV Switch 4 |
3230 |
4 |
1 |
|
Motor Thermal Capacity Used |
9630 |
0 |
8 |