Asset Management Object
Asset Management (0x6D, instance 101–199)
| Attribute ID | Name |
|---|---|
|
1 |
VendorName |
|
2 |
ProductCode |
|
3 |
MajorMinorRev |
|
4 |
VendorURL |
|
5 |
ProductName |
|
6 |
ModelName |
|
7 |
SerialNumber |
|
8 |
Time (module) ON |
|
9 |
Time Switch ON |
|
10 |
Number of event (Device Status) |
|
11 |
Number of contactor cycles |
|
12 |
Number of device power cycles |
|
13 |
Number of SIL Stops* |
|
14 |
Max I RMS |
|
15 |
Average I RMS |
|
16 |
Max Average Voltage |
|
17 |
Average Lifetime Voltage |