Control
System Control Inputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Value |
Description |
|
|---|---|---|---|---|---|---|
|
Trip Reset |
BOOL |
1 |
1 |
0, 1 |
Command
to reset an Avatar Trip Event. |
|
System Control Outputs
|
I/O Name |
Datatype |
Size (Bits) |
Scale |
Value |
Description |
|
|---|---|---|---|---|---|---|
|
System Operational |
BOOL |
1 |
1 |
0, 1 |
Indicates
that the System Avatar is in Operational mode. |
|
|
Degraded Mode |
BOOL |
1 |
1 |
0, 1 |
Indicates
that the System Avatar is in Degraded mode. |
|
|
Minor Event |
BOOL |
1 |
1 |
0, 1 |
Indicates
that the System Avatar is in Minor Event mode. |
|
|
Pre-Operational |
BOOL |
1 |
1 |
0, 1 |
Indicates
that the System Avatar is in Pre-operational mode. |
|
|
Force Mode |
BOOL |
1 |
1 |
0, 1 |
Indicates
whether the system is in Force mode. |
|
|
Test Mode |
BOOL |
1 |
1 |
0, 1 |
Returns
a status indicating that the System Avatar is in Test mode. |
|
|
IP Address |
UDINT |
32 |
— |
Max.: |
IP address of the Bus Coupler controlling the island. |
|