System Asset Management
This function block returns maintenance and product-specific information of the system device.
Modbus TCP Outputs—System Asset Management
|
Output Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Time (module) On |
28 |
0 |
32 |
|
Number of Device Events |
33 |
0 |
16 |
|
Base MAC Address |
64267 |
0 |
48 |