System Avatar
The SystemAvatar function block returns the status of the System Avatar.
Modbus TCP Inputs—System Avatar
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
Trip Reset |
8501 |
3 |
1 |
Modbus TCP Outputs—System Avatar
|
Input Name |
Address |
Starting Bit |
Size (Bits) |
|---|---|---|---|
|
System Operational |
3201 |
1 |
1 |
|
Force Mode |
3201 |
2 |
1 |
|
Minor Event |
3201 |
3 |
1 |
|
Pre-Operational |
3201 |
4 |
1 |
|
Degraded Mode |
3201 |
5 |
1 |
|
Test Mode |
3201 |
6 |
1 |
|
IP Address |
64000 |
0 |
32 |